FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Others > Number of inverters that can be connected to a 20 A branch circuit breaker
FAQ
Number of inverters that can be connected to a 20 A branch circuit breaker
The number of motors that can be connected to a 20 A branch circuit breaker for 400 V is internally defined as the total of 6.3 kW (with the maximum capacity of 2.2 kW). Is this idea also true for inverters?
- Category :
Answer
The basic idea is the same, but the total capacity should be 3.7 kW. (The maximum capacity is also 3.7K.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Others
- Series
- FR-A024