FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A100 > Inverter loss
FAQ
Inverter loss
Should I consider that the efficiency is exactly as mentioned in the material (for economy analysis)?
- Category :
Answer
The inverter efficiency changes depending on the inverter output frequency, carrier frequency, motor capacity, and load factor.
When the inverter and motor have the same capacity and are under 100% load, efficiency is 95%.
When the inverter and motor have the same capacity and are under 100% load, efficiency is 95%.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A100