FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Installation dimensions of the heat sink panel through attachment
FAQ
Installation dimensions of the heat sink panel through attachment
What are the dimensions of screw holes to attach the heat sink panel through attachment to install the heat sink externally to the FR-A520-5.5K inverter.
(Locations and sizes of the screw holes on the top and bottom surface are unknown.)
(Locations and sizes of the screw holes on the top and bottom surface are unknown.)
- Category :
Answer
The heat sink panel through attachment to the FR-A520-5.5K inverter consist of the top installation frame, bottom installation frame, and upper cover.
The top and bottom installation frame are fixed using the inverter installation holes.
Therefore, the screw hole size is M5.
The top and bottom installation frame are fixed using the inverter installation holes.
Therefore, the screw hole size is M5.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Others
- Series
- FR-A500