Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21547
  • Release Date : 2018/08/22 16:28
  • Print

Sensitivity current of earth leakage circuit breaker

The earth leakage circuit breaker NV-FA series is available for the sensitivity current 30 mA only. Can I install it on the inverter input side?
Category : 

Answer

The rated sensitivity current of the earth leakage circuit breaker can be calculated using the following equation.
If the result is 30 mA or less, the NV-FA series can be used.
(If not, you need to use a NV type with a higher rated sensitivity current.)
Product Name
Inverter, magnet motor drive
Product Category
Earth leakage circuit breaker
Series
Peripheral devices
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?