FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > Regenerative power flow
FAQ
Regenerative power flow
When multiple inverters are connected, how does the regenerative power flow?
- Category :
Answer
If all inverters are in regenerative operation, the regenerative power is regenerated to the power supply.
If one of the inverters is power driving, the regenerative power is supplied to it as the power driving power, and the rest of the regenerative power is regenerated to the power supply.
If one of the inverters is power driving, the regenerative power is supplied to it as the power driving power, and the rest of the regenerative power is regenerated to the power supply.
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option