FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Accessories and inverter with built-in high power factor converter
FAQ
Accessories and inverter with built-in high power factor converter
Do you have a product that contains the reactor 1, reactor 2, and outside box in the same case?
Also, do you have an inverter with a built-in high power factor converter?
Also, do you have an inverter with a built-in high power factor converter?
- Category :
Answer
If the reactor 1, outside box, and reactor 2 are contained in the same case as the high power factor converter, the unit becomes larger and heavier while freedom of arrangement decreases, making it harder to handle the unit. These are provided as accessories for this reason.
We do not have a product with accessories contained in the same case nor an inverter with a built-in high power factor converter.
We do not have a product with accessories contained in the same case nor an inverter with a built-in high power factor converter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option