FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Difference from conventional product (parameter unit)
FAQ
Difference from conventional product (parameter unit)
Should I use the parameter unit with the conventional inverters to change the parameters?
- Category :
Answer
The parameter unit is not available.
Use two internal potentiometers to set the electronic thermal O/L relay and acceleration/deceleration time, and two switches to set the maximum frequency.
Use two internal potentiometers to set the electronic thermal O/L relay and acceleration/deceleration time, and two switches to set the maximum frequency.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter speed controller
- Series
- SC-A