Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21601
  • Release Date : 2018/08/22 16:28
  • Print

Input terminal function selection of multi-function series

What can I do with input terminal function selection of multi-function series?
Category : 

Answer

You can use the input terminals X1 to X3 for an input terminal function such as 7-speed operation (high, middle, and low speed), output stop during motor operation with brake, and second acceleration/deceleration depending on the purpose.
Product Name
Inverter, magnet motor drive
Product Category
Common
Series
FR-U100
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?