FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Can I change the carrier frequency?
FAQ
Can I change the carrier frequency?
Can I change the carrier frequency?
- Category :
Answer
You can change it by changing the setting of Pr.72 (PWM frequency selection).
Setting range of Pr.72: 0, 1, 2, 3, 4, 5, 6 (Initial setting is "6".) (The smaller the value is, the lower the carrier frequency becomes.)
Be sure to change the carrier frequency while the inverter is stopped.
Setting range of Pr.72: 0, 1, 2, 3, 4, 5, 6 (Initial setting is "6".) (The smaller the value is, the lower the carrier frequency becomes.)
Be sure to change the carrier frequency while the inverter is stopped.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200