Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21650
  • Release Date : 2018/08/22 16:28
  • Print

Encoder

Is an encoder necessary?
If it is, what type of encoder is necessary?
Category : 

Answer

It is necessary for vector control operation. Use a dedicated motor or a motor with an encoder.
If you use another manufacturer's motor, use an encoder capable of 1000 to 4096 pulses/rotation and 5 V line driver output.
Open collector encoders are not applicable.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?