FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Encoder
FAQ
Encoder
Is an encoder necessary?
If it is, what type of encoder is necessary?
If it is, what type of encoder is necessary?
- Category :
Answer
It is necessary for vector control operation. Use a dedicated motor or a motor with an encoder.
If you use another manufacturer's motor, use an encoder capable of 1000 to 4096 pulses/rotation and 5 V line driver output.
Open collector encoders are not applicable.
If you use another manufacturer's motor, use an encoder capable of 1000 to 4096 pulses/rotation and 5 V line driver output.
Open collector encoders are not applicable.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200