FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > A7AY
FAQ
A7AY
1. Can I switch the output to current by using the A7AY while the input is 0 to 10 V?
2. Is the output current for 10 V input the rated current of the inverter?
2. Is the output current for 10 V input the rated current of the inverter?
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
1. Yes.
2. The standard set by Pr.56.
2. The standard set by Pr.56.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700