FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Full scale frequency
FAQ
Full scale frequency
A full-scale 1 mA DC analog meter is connected between the terminals FM and SD. Can I change the full-scale frequency?
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
You can change the full-scale value by changing Pr.55 (Frequency monitor reference).
The initial setting is 60 Hz.
The initial setting is 60 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700