FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Network operation
FAQ
Network operation
I am planning to operate the inverter over the network, and I want to input the start signal (STF) from the network and use an external analog signal 4 to 20 mA DC to set the frequency.
How should I set Pr.338 (Communication operation command source) and Pr.339 (Communication speed command source)?
How should I set Pr.338 (Communication operation command source) and Pr.339 (Communication speed command source)?
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
Set Pr.338 to "0" (NET) and Pr.339 to "1" or "2".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700