FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Terminal
FAQ
Terminal
The manual explains "When 4 to 20 mA current is input from the inverter terminal 4, short-circuit between AU and SD". How can I do this?
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
For an inverter with the terminal AU, use the terminal AU. For other inverters, assign the AU function to an unused terminal. And, short-circuit (turn ON) this terminal and terminal SD.
This enables frequency setting using 4 to 20 mA.
This enables frequency setting using 4 to 20 mA.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700