FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Frequency setting
FAQ
Frequency setting
I want to apply analog voltage to the inverter terminal 2, and use 0 to 5 VDC input to set the frequency to 20 Hz to 60 Hz.
How should I configure the setting?
How should I configure the setting?
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
Adjust the terminal 2 bias with Pr.C2 and Pr.C3, and the terminal 2 gain with Pr.125 and Pr.C4.
Set Pr.C2 (Terminal 2 frequency setting bias frequency) to 20 Hz and Pr.125 (Terminal 2 frequency setting gain frequency) to 60 Hz.
Set Pr.C2 (Terminal 2 frequency setting bias frequency) to 20 Hz and Pr.125 (Terminal 2 frequency setting gain frequency) to 60 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700