FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Switching between PU and NET operations
FAQ
Switching between PU and NET operations
I want to switch between the PU and NET operations
I changed Pr.340 (Communication startup mode selection) to "10" but pressing the PU/EXT button does not switch the operation mode.
After changing the parameter setting, I have not reset the power supply.
Pr.79 (Operation mode) is set to "0".
I changed Pr.340 (Communication startup mode selection) to "10" but pressing the PU/EXT button does not switch the operation mode.
After changing the parameter setting, I have not reset the power supply.
Pr.79 (Operation mode) is set to "0".
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Even after setting Pr.340 to "10", the change is reflected after resetting the power supply.
Perform the power reset.
Since changes to the communication parameters are reflected after the power reset, be sure to perform the power reset after changing them.
Perform the power reset.
Since changes to the communication parameters are reflected after the power reset, be sure to perform the power reset after changing them.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700