FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > FR-PA07
FAQ
FR-PA07
When the optional FR-PA07 is connected, is the operation command source automatically transferred to the FR-PA07?
- Category :
Answer
The operation command source is automatically transferred to the connected FR-PU07 or FR-PA07.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ