Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21708
  • Release Date : 2018/08/22 16:29
  • Print

FR-DU07

Answer

Not possible.
Instead of FR-DU07, use FR-PA07 (or FR-PU07) as an operation panel for FR-E700.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700, and others
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?