FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Coasting
FAQ
Coasting
I need the machine to coast and start up smoothly due to a load.
1. Should I set Pr.162 to "0" for this purpose?
2. How can I set the inverter for auto tuning when the "motor excitation current" is unknown?
1. Should I set Pr.162 to "0" for this purpose?
2. How can I set the inverter for auto tuning when the "motor excitation current" is unknown?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
1. Set Pr.162 to "10" (Frequency search at every start).
2. You can ignore the setting if the motor excitation current is unknown.
2. You can ignore the setting if the motor excitation current is unknown.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700