FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Parameter setting
FAQ
Parameter setting
Which parameters are necessary to set for tuning?
I use a GM-D type geared motor.
I use a GM-D type geared motor.
- Category :
Answer
Set Pr.9, Pr.71, Pr.80, Pr.81, Pr.83, Pr.84, and Pr.96.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700