FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Electromagnetic contactor
FAQ
Electromagnetic contactor
Is it fine to turn ON/OFF the electromagnetic contactor using the push button on the output side of the inverter?
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
Turning ON/OFF the output side during operation causes open/close surges that may trigger the protective function (against overcurrent or overvoltage) of the inverter or may even cause a failure. Turn ON/OFF the output side while the inverter is not operating.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700