FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Tuning
FAQ
Tuning
Although I set parameters for auto tuning, tuning was not performed and the motor rotated as usual.
How can I perform tuning?
How can I perform tuning?
- Category :
Answer
Check the parameters listed below necessary for tuning again.
Pr.9, Pr.71, Pr.80, Pr.81, Pr.83, Pr.84, and Pr.96
Pr.9, Pr.71, Pr.80, Pr.81, Pr.83, Pr.84, and Pr.96
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700