FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Automatic restart after instantaneous power failure setting
FAQ
Automatic restart after instantaneous power failure setting
Is setting Pr.162 (automatic restart after instantaneous power failure selection) enough to set the automatic restart after instantaneous power failure function?
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
You also need to set Pr.57 (Restart coasting time).
The function does not work just by setting Pr.162 unless setting this parameter.
(For A700, F700, and F700P, terminals CS and SD must be short-circuited.
Use the input terminal function assignment parameter to set the terminal CS.)
The function does not work just by setting Pr.162 unless setting this parameter.
(For A700, F700, and F700P, terminals CS and SD must be short-circuited.
Use the input terminal function assignment parameter to set the terminal CS.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700