FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Output current
FAQ
Output current
Does increasing the value of Pr.0 (Torque boost) also increase the output current?
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
Increasing the value of Pr.0 (Torque boost) increases the output voltage, and the output current also increases.
Note that increasing this value too high puts the motor in the overexcitation state, and increases the current to trigger the protective function.
Note that increasing this value too high puts the motor in the overexcitation state, and increases the current to trigger the protective function.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700