FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Frequency setting
FAQ
Frequency setting
I use the inverter's terminal 4 to input the current 4 to 20 mA DC. However, the frequency setting value gets misaligned around the middle of the input range.
Can I adjust it?
Can I adjust it?
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
You cannot calibrate the frequency around the middle of the current input range.
The inverter determines the top and bottom points in the bias/gain adjustment, links these two points with a straight line, and calculates the frequency setting value against the input current.
The inverter determines the top and bottom points in the bias/gain adjustment, links these two points with a straight line, and calculates the frequency setting value against the input current.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700