FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Frequency setting
FAQ
Frequency setting
How can I set the running frequency to 120 Hz or higher?
Use the setting dial of the inverter to set the frequency.
Use the setting dial of the inverter to set the frequency.
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
Change the value of Pr.18 (High speed maximum frequency).
You can set any frequency within the range defined by Pr.18.
You can set any frequency within the range defined by Pr.18.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700