FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Frequency setting
FAQ
Frequency setting
I input voltage of 0 to 10 V between external terminals 4 and 5 to set the frequency.
I have already changed the DIP switch setting on the board and set Pr.267 (Terminal 4 input selection) to "2".
The voltage between the terminals 4 and 5 is measured as 10 V, and the percent value of C7 (Terminal 4 frequency setting gain) is read as "101.0%". I want to set it to "100%".
Can I set it?
I have already changed the DIP switch setting on the board and set Pr.267 (Terminal 4 input selection) to "2".
The voltage between the terminals 4 and 5 is measured as 10 V, and the percent value of C7 (Terminal 4 frequency setting gain) is read as "101.0%". I want to set it to "100%".
Can I set it?
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
Since the percent value read by the calibration parameter C7 indicates that the voltage of 10 V is internally detected as 101.0%, use 101.0% as is.
If you change it to 100% unjustly, the setting frequency may rise.
If you change it to 100% unjustly, the setting frequency may rise.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700