FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Package
FAQ
Package
I found an M3 screw in the inverter package.
What is it used for?
What is it used for?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
It is the fixing screw for the inverter cooling fan cover.
The size and number of screws depend on the model and capacity.
(When exporting the product to the EU, this screw fixes the fan cover so that it would not come off during transport.
It is not necessary when the product is used in Japan.)
The size and number of screws depend on the model and capacity.
(When exporting the product to the EU, this screw fixes the fan cover so that it would not come off during transport.
It is not necessary when the product is used in Japan.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700