FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Auto tuning
FAQ
Auto tuning
I use the geared motor GM-DZG. Which value should I set to Pr.71 (Applied motor) for auto tuning?
- Category :
Answer
Set it to "13" (Constant-torque).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-A700