FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Advanced magnetic flux vector control
FAQ
Advanced magnetic flux vector control
I want to operate the inverter using Advanced magnetic flux vector control.
What setting is required?
What setting is required?
- Category :
Answer
To use Advanced magnetic flux vector control, basically set Pr.9, Pr.80, Pr.81, Pr.71, and Pr.800.
Auto tuning is necessary in some cases. Set Pr.83, Pr.84, and Pr.96 in addition to above for it.
Set these parameters and perform tuning.
Auto tuning is necessary in some cases. Set Pr.83, Pr.84, and Pr.96 in addition to above for it.
Set these parameters and perform tuning.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700