Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21756
  • Release Date : 2018/08/22 16:29
  • Print

Advanced magnetic flux vector control

I want to perform Advanced magnetic flux vector control using the geared motor GM-S(B).
Which value should I set to Pr.71 (Applied Motor)?
Category : 

Answer

When using the geared motor GM-S(B), set Pr.71 to "13" and also set Pr.9, Pr.80, and Pr.81.
Perform auto tuning as required. Perform auto tuning as required. Settings of Pr.83, Pr.84, Pr.96, and Pr.800 are also required to be configured.
Set these parameters and perform tuning.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?