FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Monitor indicator
FAQ
Monitor indicator
I want to check the frequency on the monitor but when I set the running frequency and operate the inverter, the monitor shows the current (A).
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
The first priority window of the monitor may be set to the current.
When the current is displayed on the monitor (the unit is "A"), press "SET" to switch to the voltage monitor window (no unit), and then press "SET" again. The frequency is shown on the monitor (the unit is "Hz").
If you want to set the frequency as the first priority, press and hold the "SET" key for a while.
When the current is displayed on the monitor (the unit is "A"), press "SET" to switch to the voltage monitor window (no unit), and then press "SET" again. The frequency is shown on the monitor (the unit is "Hz").
If you want to set the frequency as the first priority, press and hold the "SET" key for a while.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700