FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Program command
FAQ
Program command
Initially, the program for checking the data link status is input as an example. Is it necessary to input it each time a new command (monitor or parameter setting) is input?
- Category :
Answer
This subroutine is to check the data link status and needs to be executed only once at the start of the program.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700