Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21769
  • Release Date : 2018/08/22 16:29
  • Print

Parameter

Is there any parameter that can be used to change the time before an overload trip (electronic thermal O/L relay error) occurs?
Category : 

Answer

No parameter can be used to directly set this time.
Changing Pr.9 (Electronic thermal O/L relay) changes the time.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?