FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Multi-speed setting
FAQ
Multi-speed setting
What are the priorities between multi-speed settings?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Priorities are: Low speed (RL) > Middle speed (RM) > High speed (RH).
For example, if the low speed (RL) and middle speed (RM) signals are input simultaneously, the low speed (RL) signal is prioritized.
For example, if the low speed (RL) and middle speed (RM) signals are input simultaneously, the low speed (RL) signal is prioritized.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700