Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21781
  • Release Date : 2018/08/22 16:29
  • Print

Output frequency monitor value

After performing auto tuning, the output frequency monitor value was higher than the setting frequency at the operation.
Why is this?
How can I return the inverter to V/F control?
Category : 

Answer

When running the inverter after auto tuning, the frequency setting value is increased by the amount of the motor slippage, resulting in a higher monitor value.
To return to V/F control, return Pr.80 (Motor capacity) and Pr.811(Number of poles) to "9999".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries