FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Frequency setting
FAQ
Frequency setting
I want to operate the inverter with up to 80 Hz by an external potentiometer.
I changed Pr.3 (Base frequency) to "80 Hz", but the running frequency did not rise.
How should I configure the setting?
I changed Pr.3 (Base frequency) to "80 Hz", but the running frequency did not rise.
How should I configure the setting?
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
Since Pr.3 (Base frequency) is a parameter to set the rated motor frequency, setting it to 80 Hz does not increase the frequency.
Set this parameter to the rated frequency.
To increase the running frequency, set Pr.125 (Terminal 2 frequency setting gain frequency) to "80 Hz".
Set this parameter to the rated frequency.
To increase the running frequency, set Pr.125 (Terminal 2 frequency setting gain frequency) to "80 Hz".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700