FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Frequency setting
FAQ
Frequency setting
I want the inverter to start at low speed (RL) when an external signal is input and then I want to set the frequency using the setting dial on the operation panel after the external signal is turned off.
The inverter is started by short-circuiting the terminals STF and SD.
The inverter is started by short-circuiting the terminals STF and SD.
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Set Pr.79 (Operation mode) to "3".
When a signal is input to the terminal RL, the inverter starts operating at the frequency set with Pr.6 (Multi-speed setting, low speed) (initially set to 10 Hz). The frequency set using the setting dial becomes effective when the RL signal is turned off.
When a signal is input to the terminal RL, the inverter starts operating at the frequency set with Pr.6 (Multi-speed setting, low speed) (initially set to 10 Hz). The frequency set using the setting dial becomes effective when the RL signal is turned off.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700