FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Frequency setting
FAQ
Frequency setting
I use the setting dial to set the frequency. The frequency changes when I turn the dial, but it returns to the previous value after flickering for several seconds.
I want to change the frequency just by turning the setting dial.
I want to change the frequency just by turning the setting dial.
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
Change Pr.161 (Frequency setting/key lock operation selection) to "1" (potentiometer mode).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700