FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Frequency setting
FAQ
Frequency setting
I set the frequency to 10 Hz because I wanted to operate the motor at 10 Hz.
When I started the inverter in Advanced magnetic flux vector control, a frequency 10 Hz higher than the setting was output. What is wrong with the inverter setting?
When I started the inverter in Advanced magnetic flux vector control, a frequency 10 Hz higher than the setting was output. What is wrong with the inverter setting?
- Category :
Answer
When running the inverter in Advanced magnetic flux vector control, the frequency setting value is increased by the amount of the motor's slippage, resulting in a higher frequency than commanded. It is not a fault.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700