FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Frequency setting
FAQ
Frequency setting
Which parameter is used to set the maximum frequency when setting the frequency with the setting dial?
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
Pr.1 (Maximum frequency) or Pr.18 (High speed maximum frequency).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700