FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Frequency meter
FAQ
Frequency meter
While the inverter monitor shows 60 Hz, the external frequency meter shows 30 Hz. I want to adjust this misalignment.
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
First, check if Pr.55 (Frequency monitor reference) that is the reference for the FM output is set correctly.
Next, operate the inverter (without connecting a motor) at the specified frequency, and adjust the value of the calibration parameter C0 by turning the setting dial while checking the frequency meter.
Next, operate the inverter (without connecting a motor) at the specified frequency, and adjust the value of the calibration parameter C0 by turning the setting dial while checking the frequency meter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700