FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Programmable controller
FAQ
Programmable controller
While I want to input the inverter output frequency into the programmable controller as an analog signal, the terminal FM is pulse output and cannot be input directly.
Is there an option to input it directly?
Is there an option to input it directly?
- Category :
Answer
Please use the inverter optional FR-A7AY.
It supports voltage output (0 to 10 VDC) and current output (0 to 20 mA DC).
For the voltage output (0 to 10 VDC), the terminal AM of the inverter supports the A700/F700(P).
It supports voltage output (0 to 10 VDC) and current output (0 to 20 mA DC).
For the voltage output (0 to 10 VDC), the terminal AM of the inverter supports the A700/F700(P).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700