FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > External terminal
FAQ
External terminal
I want to implement start self-holding using the external terminal "RL".
1. Should I use the external terminal STF and the terminals RL and SD?
2. Which value should I set to Pr.180 (RL terminal function selection)?
1. Should I use the external terminal STF and the terminals RL and SD?
2. Which value should I set to Pr.180 (RL terminal function selection)?
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
1. Use the external terminals STF, RL, and SD. (A push-ON switch for operation is required between the terminals STF and SD, and a push-OFF switch is required between the terminals RL and SD. For the detailed wiring, refer to the Instruction Manual.)
2. Set Pr.180 to "25" (Stop self-holding selection).
2. Set Pr.180 to "25" (Stop self-holding selection).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700