FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Operation mode setting value
FAQ
Operation mode setting value
When inputting the start command and frequency setting command for operation externally, which value should be set to Pr.79 (Operation mode)?
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
Set Pr.79 to "2" (external operation mode).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700