FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > CC-Link
FAQ
CC-Link
In CC-Link operation, is it possible to monitor the running frequency and output current simultaneously?
- Category :
Answer
Yes. Set the first monitor code in the lower 8 bits and the second monitor code in the upper 8 bits of RWwn.
Set H6F to the first monitor code, and H70 to the second monitor code.
Set H6F to the first monitor code, and H70 to the second monitor code.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700