FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > CC-Link
FAQ
CC-Link
I consider performing CC-Link operation. Can the operation (start) commands be input both from PU and NET?
- Category :
Answer
The start commands cannot be input from both sources simultaneously because the operation command source is specified.
You can switch the command source as necessary.
You can switch the command source as necessary.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700