FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > CC-Link
FAQ
CC-Link
I perform CC-Link operation. While Pr.544 (CC-Link extended setting) is set to "12" for double setting, should I set it to quadruple setting to check the fault records?
- Category :
Answer
You can check the fault records with Pr.544 (CC-Link extended setting) set to "12" for double setting.
Set H74 for the instruction code and turn ON RYF.
Set H74 for the instruction code and turn ON RYF.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700