FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > CC-Link
FAQ
CC-Link
Is it necessary to change Pr.544 (CC-Link extended setting) to check parameters No.100 and later on CC-Link?
How can I input the instruction code for link parameter extended setting?
How can I call link parameter extended setting?
I want to change Pr.544 to "1" in the NET mode of CC-Link operation. I used the operation panel FR-DU07 to change Pr.544 to "1" but I could not read the parameters No.100 and later.
How should I configure the setting?
How can I input the instruction code for link parameter extended setting?
How can I call link parameter extended setting?
I want to change Pr.544 to "1" in the NET mode of CC-Link operation. I used the operation panel FR-DU07 to change Pr.544 to "1" but I could not read the parameters No.100 and later.
How should I configure the setting?
- Category :
Answer
If Pr.544 (CC-Link extended setting) is set to other than "0", you do not need to change Pr.544 (CC-Link extended setting).
Write the extended setting of the instruction code written in the parameter list in the Instruction Manual (Applied), to the upper 8 bits and the read code to the lower 8 bits of RWw2.
If Pr.544 remains in the initial setting ("0"), an extension program is necessary.
After running the program for the link parameter extended setting, run the program for the parameters to set.
To enable the change of Pr.544, you need to reset the inverter after changing it.
Write the extended setting of the instruction code written in the parameter list in the Instruction Manual (Applied), to the upper 8 bits and the read code to the lower 8 bits of RWw2.
If Pr.544 remains in the initial setting ("0"), an extension program is necessary.
After running the program for the link parameter extended setting, run the program for the parameters to set.
To enable the change of Pr.544, you need to reset the inverter after changing it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700